system
July 30, 2024, 10:36am
1
Animations allows to visualize state of equipment in a model by applying the visual effects to a model object. There are following animation types are supported:
This is a companion discussion topic for the original entry at https://developer.siemens.com/building-x-openness/api/lifecycletwin-api/examples/animations/model-animations.html
I successfully created a variable using POST/variables.
{
“Id": "00000000-0000-0000-0000-000000000000",
"Name": "Reservation Status: 29A Meeting Room",
"Key": "Reservation Status: 29A Meeting Room",
"Type": 8,
"NumericValue": 0.0,
"StringValue": ""
}
I successfully created an animation using POST/models/animations/raw
{
"Name": "Reservation Status: 29A Meeting Room",
"Definition": "{\"Models\": [{\"Id\": \"a119a348-15b7-3502-9df7-5e109ed4ce8c\", \"Ids\": [\"3tVs6ewnP158K_JdR9viCB\"]}], \"Animations\": [{\"Conditions\": [{\"RDSVar\": \"Reservation Status: 29A Meeting Room\", \"Type\": \"Equal\", \"Value1\": 4}], \"LogicalOperation\": \"AND\", \"AnimationType\": \"Color\", \"Parameters\": \"{\\\"Speed\\\": 5.0, \\\"Color\\\": \\\"#FF0000\\\"}\", \"IsBlinked\": true}]}",
"Id": "00000000-0000-0000-0000-000000000000"
}
I can successfully modify the variable value using PUT/variables/{{varGuid}}
But after this, the animation is not working. What/where did I go wrong?