I use ix-select inside a grid and when I click on it, the values are shown “behind” other elements in the table. It seems if I do it on the first few rows, it doesn’t work, but on the last row it does show fine (probably because no other elements below it, also can work for more line at the end of the table).
Same thing happens with ix-dropdown, as can be seen below.
I’m using version 30.2.1 of AG Grid Angular, those are the other relevant versions for IX:
“@siemens/ix”: “^2.4.1”,
“@siemens/ix-aggrid”: “^2.1.6”,
“@siemens/ix-angular”: “^2.4.1”,
“@siemens/ix-icons”: “^2.2.0”,